Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Z-Slide8

The following slides are examples of applications that will take advantage of the characteristics of the Z-Match capacitors which were previously explained. The first application is an impedance matching application used in RF circuits in the PA, LNA or antenna section. The matching circuits used in communication equipment generally require narrow tolerance, high-Q factor and high SRF. By utilizing Z-Match, it is possible to design performing circuits that result in low noise, high gain and reduced power loss.

PTM Published on: 2011-09-15